A comprehensive portfolio of SURF products for Oil & Gas

A comprehensive portfolio of SURF products for Oil & Gas


We’re intent on keeping pace with industry trends. And we’re always listening to what our customers require, whilst anticipating their future needs.

 

So we know a thing or two about the specialised needs of Oil & Gas operators. But to ensure we continued to meet and even anticipate our customer’s developing needs with the latest in technological support, we performed an assessment of where the industry is moving, both in Brazil and in larger global markets. And the data gathered enabled us to identify areas for development.

Our SURF team, led by Rafael Tanaka, Engineering Manager in Brazil, evolved their current designs, applications methodology and factory processes.

The result? Prysmian’s STU. 

A product range inspired by our customers

Designed and manufactured in our SURF units located at Cariacica and Vila Velha, Brazil, the prototype was produced and tested during July 2016.

It marks a further addition to our now fully comprehensive portfolio of SURF (Subsea Umbilical, Riser and Flowline) products for applications in offshore exploration activities and the petrochemical industry.

Prysmian’s STU offers the highest performance levels at the deepest depths. 

Guaranteeing the best

At Prysmian, we continually and rigorously test our SURF technologies to deliver the best performing products on the market.  So we aren’t finished yet.

The next phase of the development will include installation of ancillaries and full-scale testing, as would typically be required by the customer prior to field installation.

This is an important milestone for Prysmian O&G that will allow us to differentiate our products portfolio from the competition whilst better serving both the Brazilian and export markets”. 

Cristiano Tortelli

Senior Vice President Oil & Gas

Turnkey service provider

We offer a full range of SURF solutions for the Oil & Gas sector. But we offer so much more… Product innovation and partnership lie at the heart of our SURF business.

So we work closely with our customers to determine their needs and challenges, ensuring that our products and services can help to solve any umbilicals issues they may have.

What’s more, our decades of engineering experience and our global footprint mean:

  • We can deliver a competitively extensive portfolio for the Oil & Gas sector
  • We’re about more than products. We offer a whole host of services to our customers – from installation to after-sales support
  • We can be as flexible as our customers require

Building on a history of milestones in umbilicals

Over the years, we’ve innovated significantly in the SURF sector. For example, we achieved the following milestones in terms of water depths achieved:

  • 1994 for the Petrobras Marlim field (MRL-4, approximately 1000 m WD)
  • 2003 for the Petrobras Roncador field (RO-21, approximately 1886 m WD)
  • 2014-2015 for the Sapinhoa field reaching 2500 m WD in the pre-salt application.

Bringing state-of-the art and comprehensive technology to the market remains our primary goal and we’ll continue to use our customers and the wider industry as the benchmark for future developments.

EN - Stories - Magazine

Id: 3957

Type: panel

Url: node/3957